SCADAPack x70

Configure the Data Logging Settings

The Settings tab on the Forms of SCADAPack x70 Device Configuration items includes a Data Logging section. The properties in this section are only available for use if the Data Logging option is enabled (see Configure the Device Options). Use the Data Logging section to configure the required data logging settings. Data logs are stored on the SCADAPack x70 device according to the data log configurations and the data logging requirements specified for each Analog, Digital, and/or Counter Configuration item on the SCADAPack x70 device.

Use the following settings to configure the data logging feature:

Internal Drive Space

Specify the maximum amount of internal file system drive space that the Data Logging feature is to use in the SCADAPack x70 device. The valid range, in kilobytes, is from 512 to 51200 KB (inclusive). The default value is 1024 KB.

This field is applicable only if you configure the data logs to be saved to the internal drive (see Configure a SCADAPack x70 Data Log Item).

Log Initial Value Events

Select the check box if an event representing the value (the initial value) for each object is to be logged each time a new file is created in the data log.

Clear the check box if no events are to be logged. This is the default setting.


Disclaimer

Geo SCADA Expert 2022