SCADAPack x70

Specify the Data Logging Requirements - Counter Configuration

The SCADAPack x70 tab on the Forms of SCADAPack x70 Counter Configuration items contains a Data Logging section. Use the section to specify the data log and the required events that are to be logged for the SCADAPack x70 Counter Configuration item. The properties in the section are only available for use if the SCADAPack x70 Device Configuration item with which the Counter Configuration item is associated has Data Logging enabled (see Configure the Device Options).

Use the following settings:


Disclaimer

Geo SCADA Expert 2022