Import/Upload Summary
Associated with: SCADAPack x70 Device Configuration items.
The Import/Upload Summary status attribute provides a summary of the latest import of a configuration file from RemoteConnect, or upload of the configuration from a SCADAPack x70 device.
There are three different stages of an import/upload transaction. The Import/Upload Summary status attribute displays different values at each stage:
- Stage 1: Transaction Queued
When the import/upload transaction is queued, the status attribute displays the following value:
SCADAPack x70 import configuration transaction queued at <date> <time>, Waiting
- Stage 2: Transaction in Progress
This stage of the transaction progresses in three phases. They are:
- Updating the database items, when the following information is displayed:
SCADAPack x70 import configuration transaction queued at <date> <time>, Processing... Updating
-
Marking for possible deletion any redundant database items. This comprises setting database items for which no match is found in the imported/uploaded configuration as Out of Service.
The following information is displayed:
SCADAPack x70 import configuration transaction queued at <date> <time>, Processing... Deleting
-
Finalizing the transaction, when the following information is displayed:
SCADAPack x70 import configuration transaction queued at <date> <time>, Processing... Finalizing
The actual activities that occur during this stage of an import/upload vary depending on:
- The selected Mode
- The differences between the configuration that is being imported/uploaded and any existing database items associated with the SCADAPack x70 device.
- Updating the database items, when the following information is displayed:
- Stage 3: Transaction Completed
When the import/upload is completed, the status attribute displays the following value:
SCADAPack x70 import configuration transaction queued at <date> <time> completed
If an import or upload succeeds with warnings, or if Geo SCADA Expert is unable to import or upload configuration for a SCADAPack x70 device, a configuration report is created (see Configuration Reports for SCADAPack x70 Devices).
Use this status attribute alongside the Import/Upload Status status attribute to monitor the progress of an import/upload transaction.
Further Information
For further information about the activities that occur when an import or upload is in progress, see the following topics: