Uninstalling Geo SCADA Expert

There are two different ways of uninstalling Geo SCADA Expert:

To discover which of the uninstall processes is most appropriate for your requirements, answer the questions below:

  1. Do you intend to re-install Geo SCADA Expert on the computer at a later date?
  2. Do you want a re-installed version of Geo SCADA Expert to use only the default settings (that is, be a ‘clean’ install)?

If you answered no to any of the questions, we recommend that you use the ‘Quick’ uninstall process (see Uninstall Geo SCADA Expert - ‘Quick’ Uninstall).

If you answered yes to both of these questions, you should use the ‘Complete’ uninstall process (see Uninstall Geo SCADA Expert - ‘Complete’ Uninstall). But to do so, you need to have experience of editing registry settings in Windows. This is because incorrect configuration of the registry can cause serious problems with the Windows operating system.

To perform a complete uninstall, you need to also uninstall the Virtual ViewX component, which is installed separately from Geo SCADA Expert, (see Uninstall Virtual ViewX).

To ensure a clean uninstallation of Geo SCADA Expert components, make sure that you uninstall Geo SCADA Expert before you uninstall any IIS components or the Crystal Reports runtime.


Disclaimer

Geo SCADA Expert 2022