Points Used on TBox Outstations

A TBox outstation supports a combination of the following points for collecting data and controlling equipment:

For general information about Points in Geo SCADA Expert, see Introduction to Points in the Geo SCADA Expert Guide to Core Point Configuration.

You need to configure one point of the appropriate type on the outstation for each register (tag) on an RTU for which data retrieval or control is required. Configure the properties for each point using the appropriate TBox Point Form. The Forms have several tabs (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

For the minimum configuration required to create a functioning TBox point in Geo SCADA Expert, see Minimum Configuration for a TBox Point.

For the common properties of TBox points, see Configure Common Point Properties.

For an Output point, there is an option to report the value immediately after a control action has been carried out: see Specify Whether to Update an Output Point Value Immediately Following a Control Action.

 


Disclaimer

Geo SCADA Expert 2022