TREND Optional Values
            Place any optional TREND values outside of any other sections, but within the TREND section in a TrendSpec definition. Remember to include a comma before listing any of these optional values. Include a comma between each optional value’s definition.
Many of the optional TREND values are equivalent to the properties that you can specify using the Trend Properties window on a Pre-Configured Trend. For further information on these properties, see Configure the Display Settings for a Trend.
The optional values that you can specify within the TREND section are:
| 
                                 TREND Optional Values  | 
                        ||
|---|---|---|
| 
                                 Identifier  | 
                            
                                 Value Type  | 
                            
                                 Comments  | 
                        
| 
                                 Title (Use as an alternative to the TitleExpr identifier.)  | 
                            
                                 String  | 
                            
                                 Use to define the Trend’s title. Example: Title = 'Sensor1' Alsosee Use TrendSpec to Define a Multiple Trace Ad Hoc Trend. To use an expression to define the value of the Trend’s title, use the TitleExpr identifier instead of this Title identifier.  | 
                        
| 
                                 ShowYAxes  | 
                            
                                 Boolean  | 
                            
                                 Use to specify whether any y-axes are shown on the ad hoc Trend. (You need to include a YAXIS section per trace in your TrendSpec definition, regardless of the value of the ShowYAxes identifier.) Example: ShowYAxes = True If an ad hoc Trend is multi-trace and y-axes only need displaying for some of those traces, omit the TREND ShowYAxes identifier and include individual YAXIS Visible identifiers in your TrendSpec definition.  | 
                        
| 
                                 ShowXAxis  | 
                            
                                 Boolean  | 
                            
                                 Use to specify whether the x-axis is shown on the ad hoc Trend. (You need to include an XAXIS section in your TrendSpec definition, regardless of the value of the ShowXAxis identifier.) Example: ShowXAxis = True  | 
                        
| 
                                 ShowTitle  | 
                            
                                 Boolean  | 
                            
                                 Use to specify whether the Trend Title is shown on the ad hoc Trend. Example: ShowTitle = True Geo SCADA Expert only takes into account the values of any other Title identifiers if ShowTitle = True.  | 
                        
| 
                                 ShowKey  | 
                            
                                 Boolean  | 
                            
                                 Use to specify whether the Trend Key is shown on the ad hoc Trend. Example: ShowKey = False  | 
                        
| 
                                 TitleExpr (Use as an alternative to the Title identifier.)  | 
                            
                                 String  | 
                            
                                 Use to define the Trend’s title. Example: TitleExpr = '''AdHocTrends.Sensor1''' Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes. To specify a string, rather than an expression, use the Title identifier instead of this TitleExpr identifier.  | 
                        
| 
                                 AlarmLimitLabelPos  | 
                            
                                 Identifier value  | 
                            
                                 Use to specify the position of the alarm limit labels. Specify one of these values: LimitLabelNone, LimitLabelAboveLeft, LimitLabelAboveRight, LimitLabelOverLeft, LimitLabelOverRight, LimitLabelLeft, or LimitLabelRight Example: AlarmLimitLabelPos = LIMITLABELABOVERIGHT Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                
                                 TitleColour  | 
                            
                                 RGB  | 
                            
                                 Use to specify the RGB color that is assigned to the Trend’s title. Example: TitleColour = RGB(0,0,0)  | 
                        
| 
                                 TitleFont  | 
                            
                                 String  | 
                            
                                 Use to specify the font used for the Trend’s title. Example: TitleFont = 'Tahoma' Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 TitleFontHeight  | 
                            
                                 Integer  | 
                            
                                 Use to specify the height of the font used for the Trend’s title. Example: TitleFontHeight = 8 Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 TitleFontStyle  | 
                            
                                 Identifier value or Integer  | 
                            
                                 Use to specify the attributes assigned to the Title’s text. For information on the values that you can specify, see Supported FontStyle Identifier and Integer Values. Example: TitleFontStyle = FontStyleBold or TitleFontStyle = 1 Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 MainFont  | 
                            
                                 String  | 
                            
                                 Use to specify the font used for the text that is shown in the main body of the Trend window. Example: MainFont = 'Tahoma' Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 MainFontHeight  | 
                            
                                 Integer  | 
                            
                                 Use to specify the height of the font used for the Trend’s body text. Example: MainFontHeight = 8 Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 MainFontStyle  | 
                            
                                 Identifier value or Integer  | 
                            
                                 Use to specify the attributes assigned to the Trend’s body text. For information on the values that you can specify, see Supported FontStyle Identifier and Integer Values. Example: MainFontStyle = FontStyleRegular or MainFontStyle = 0 Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 LabelFont  | 
                            
                                 String  | 
                            
                                 Use to specify the font used for the y-axes’ label. Example: LabelFont = 'Tahoma' Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 LabelFontHeight  | 
                            
                                 Integer  | 
                            
                                 Use to specify the height of the font used for the y-axes’ label. Example: LabelFontHeight = 8 Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                 LabelFontStyle  | 
                            
                                 Identifier value or Integer  | 
                            
                                 Use to specify the attributes assigned to the y-axes’ label’s text. For information on the values that you can specify, see Supported FontStyle Identifier and Integer Values. Example: LabelFontStyle = FontStyleBoldItalic or LabelFontStyle = 3 Alsosee Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.  | 
                        
| 
                                
                                 BackgroundColour  | 
                            
                                 RGB  | 
                            
                                 Use to specify the RGB color used for the ad hoc Trend’s background. Example: BackgroundColour = RGB(236,233,216)  |