Change your Password

ATTENTION: This section only applies to User Accounts that are managed directly in Geo SCADA Expert. With User Accounts that are associated with Windows or LDAP User Profiles, password management is performed via the relevant Windows domain or LDAP server.

It is important that you keep your password secret. If another user logs in using your user name and password, any actions they perform will be logged against your name. If you think that your password has been compromised, you should change it.

You have to be logged on to Geo SCADA Expert to change your password (see Log On to ViewX). You can change your password if your user account has the Can Change Password feature enabled and is not authenticated via Windows or LDAP. Check with your system administrator.

To change your user password when you are logged on to Geo SCADA Expert:

  1. Select the Home tab on the ViewX ribbon.
  2. Select the Change Password tool command from the relevant command group.

    The Change Password window is displayed.

    If you are using a ViewX client connected to two or more systems, the Change Password command includes a drop-down menu from which you can select to change the password for a particular system, or all systems.

    If you use this menu, your selection displays in the System field on the Change Password window when it appears.

    You can also display the Change Password window by selecting the Change Password option from your user account’s context sensitive Object Menu. You can display the menu from, for example, your user account’s entry in the Database Bar.

  3. The System field allows you to change your password for one specific system or All Systems simultaneously. Choose an option from the field’s drop-down list, which comprises the Geo SCADA Expert systems (databases) to which the ViewX client has access.
  4. Enter your existing password in the Old Password field. This is only required if your user account does not have the Security permission for the User item. If your user account does have the Security permission for the User item, the Old Password field is ‘grayed out’ and unavailable for use.
  5. Enter your new password in the New Password field. The field is case-sensitive.
  6. Enter the new password again in the Confirm Password field.
  7. Select the OK button to confirm the change.
    If the password change is successful, the Change Password window is closed and the new password is applied to the specified user account.

    If the password change is not successful, the Change Password window will display a message explaining the problem that occurred.

    If this occurs, take note of the reason(s) given and select OK to attempt to change the password again.


Disclaimer

Geo SCADA Expert 2022