Log On to ViewX

For security, Geo SCADA Expert has user accounts. Designed to be allocated to individual members of staff, user accounts have:

Typically, to access ViewX, you need to log on by entering a valid user name and password. If you do not log on via a user account, Geo SCADA Expert might log you on as the Guest user automatically. The Guest user is a built-in user account that, if active on your system, might be configured to provide very limited access to Geo SCADA Expert (see Guest User Account and Everyone User Group).

To log on to ViewX via a user account:

  1. Display the Log On window. There are several ways of doing this:
    • Select the Home tab on the ViewX ribbon. Select Log On from the Security command group.

      This displays a Log On window that allows you to log on to one or more systems simultaneously.

      If you are connected to two or more systems, the Log On command includes a drop-down menu from which you can select to log on to a particular system, or all systems.

      If you use this menu, your selection displays in the System field on the Log On window when it appears.

    • In the Database Bar, right-click on the system you want to log on to, and then select the Log On option from the context sensitive menu. This displays the Log On window with the selected system displayed in the System field.

    • Select the Log On command to the right of the ViewX title bar. This displays the Log On window.

      This command is only available if no one is logged on and the Guest user account is active. If this is the case, the command will display a key icon.

    • Select the Log On option from any other display, for example, from a Mimic that provides a hyperlink to the Log On window for the system.
  2. When you have displayed the Log On window, you need to enter the following information:
    • System—You can choose to log on to one specific system or to log on to All Systems simultaneously (see Multiple Databases). The field’s drop-down list comprises the Geo SCADA Expert systems (databases) to which the ViewX client has access.

      When logging on to multiple systems, Geo SCADA Expert attempts to log you on to all of the systems (databases) to which it has access, using the same user name and password. If the user name and password are invalid for a system, a diagnostic message is displayed. You will need to log on to that system individually.

    • User Name—Enter your unique user name. This is the user name that has been configured for your user account.

      If your system is configured to use the External Authentication feature, a system administrator will be able to advise you as to whether your user name for ViewX is the same as your Windows or LDAP user name.

    • Password—Enter the password for your user account. If you are unsure of the password, please contact a system administrator.

      If your system is configured to use the External Authentication feature, your password for ViewX will be the same as your Windows or LDAP password. For more information about the feature, see Using External Authentication with Geo SCADA Expert.

      If your user account is managed directly in Geo SCADA Expert and you attempt to log on to multiple systems (databases) simultaneously and use a password that has expired on one or more of the systems, the Change Password window is displayed. You will need to change the password (see Change your Password). The new password is applied to your user account on all systems on which your user account exists and to which the ViewX client has access. The password expiry times begin again starting from the time you set the new password (see Define the Default Security Settings for New User Accounts).

      (If your system is configured to use the External Authentication feature and your user account is associated with a Windows or LDAP User Profile, password changes are managed via the relevant Windows or LDAP server.)

    On a ViewX workstation on which the On-Screen Keyboard feature is enabled, an alphanumeric keyboard is displayed whenever the User Name or Password fields are selected. You can use either a traditional keyboard or Use the Use the Alphanumeric Touch Screen Keyboard to enter your Username and Password.

  3. Select the OK button.
    If the log on is successful, the Log On window is closed and you are logged on to the selected system(s).

    If the log on is not successful, the Log On window will display a message explaining the problem that occurred.

    If this occurs, take note of the reason(s) given and select OK to attempt to log on again.

    If you attempt and fail to log on multiple times the system may disable your account temporarily for a specified duration. If the system is configured to limit the number of failed log on attempts your account may become disabled permanently, (see Define the Default Security Settings for New User Accounts). The password will need to be reset if it has been permanently disabled, (see Define the Password for a User).

    The systems to which you are logged on are displayed by the Log On Status field to the far right of the ViewX title bar. If you use the same user name to log on to all of the systems offered, the Log On Status displays that user name. If you use different user names to log on to different systems, the drop-down menu on the Log On Status displays a list of user names and the system to which they apply in the format:

    <System>: <Username>

    Example:

    If you are logged in to two or more systems with different non-guest user accounts, the Log On Status will display "Multiple Users".

In the unlikely event that logging on causes unexpected ViewX behavior, you may need another user to reset the profile for your user account, see Reset Profile.


Disclaimer

Geo SCADA Expert 2022