Configuring Digital Points

Use Advanced EWS Digital Points to map digital ‘point’ data on Advanced EWS servers into ClearSCADA in a suitable format, and vice versa.

Configure the properties of each Digital point using the fields on the Advanced EWS Digital Point Form.

This section covers configuration of the digital-specific properties on the Digital Point tab of the Form.

Use the Digital Point tab to:

For information about the Digital Point tab on the Digital Point Form, see Defining Digital Point Details in the ClearSCADA Guide to Core Point Configuration.

If the point is a digital output point:

Properties on other tabs are common to many points, see Tabs on Point Forms in the ClearSCADAGuide to Advanced Drivers.


Disclaimer

ClearSCADA 2017 R2