Decide When ClearSCADA is to Execute a System Command

ClearSCADA can trigger a system command under various circumstances. You need to decide when ClearSCADA is to execute each system command, in order to determine the type of configuration that you need to undertake:

In addition to the above, ClearSCADA is supplied with a built-in command line tool, to enable third-party applications to run ClearSCADA commands from the Windows® command prompt. For more information, see Server Command Line Tool in the ClearSCADA Guide to Server Administration.


Disclaimer

ClearSCADA 2017 R2