Secondary Window Container
Secondary Window Containers display document windows in Run Mode or Design Mode, allowing database items such as Mimics, Lists, Trends or reports to appear simultaneously on separate monitors. A Multi-Monitor setup supports up to 5 Secondary Window Containers.
You can configure a Secondary Window Container to:
- Display a single document
- Display multiple documents (if your user account provides access to a Multi Document Interface) (see Define the ViewX Configuration Settings for a User).
If a container supports multiple documents, each document window appears with its own tab.
Secondary Window Containers can also display the Alarm Banner or they can be configured to display the Alarm Banner in Full mode (see Launch the Alarm Banner to Fill Container Mode).