Launch the Crystal Reports Application

To launch the Crystal Reports application from within ClearSCADA, either:

  1. Double-click on the Report entry within the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature).

Or:

  1. Either:
  2. or:

    or:

  3. Select the Edit Crystal Reports option.

The Crystal Reports application window overlays the ClearSCADA window (see Understand the Crystal Reports Work Areas).


Disclaimer

ClearSCADA 2017 R3