Previous Update Status

Associated with: Points

This status attribute displays information about a point’s status at the time that it was Previously Updated in ClearSCADA (as opposed to its Current Status).

Possible Status values might include:

Use the attribute in conjunction with other status attributes, such as Previous Update Quality, to assess the reliability of the data.

Also see Previous Update Value.

Use the State Change Status attribute to determine the point status that applied before the point changed to its Current State.


Disclaimer

ClearSCADA 2017 R3