Put Aside Status

Associated with: Points for which a local Override is currently in force

This status attribute displays the point status that was ‘put aside’ at the time that the current local Override came into force.

Use the attribute in conjunction with the other Put Aside status attributes (such as Put Aside Value, Put Aside Quality, and Put Aside Last Updated) to ascertain further information about the point data that was ‘put aside’.

For information about the values that the Put Aside Status attribute might display, see Previous Update Status.


Disclaimer

ClearSCADA 2017 R3