Display the Layers Window

To add, remove, or reorder the layers for a Mimic, you need to access the Layers window.

To access the Layers window:

  1. Display the Mimic you want to edit in Design mode.
  2. Select Layers in the View command group on the Graphics Tab.

    The Layers window will display.

The Layers window contains a list of the layers that are already set up for the Mimic (if any). Information about the layers is shown in the following categories:

The Layers window also contains the following buttons:


Disclaimer

ClearSCADA 2017 R3