Differences Between the WebX Client and ViewX

WebX is available as the newer web server hosted using IIS and installed separately from the ClearSCADA server, or the Original WebX server built in to each ClearSCADA server instance. This topic refers to both versions, using the terms 'Original WebX' and 'WebX (the newer web server hosted using IIS)' where there are differences, and 'WebX' where they are the same.

Many of the functions and displays that are available from a ViewX client are also available from a WebX client:

The differences in how you use a WebX client compared with ViewX mostly relate to how you access items and functions.

ATTENTION: WebX uses Microsoft ActiveX Controls technology to display various types of document. ActiveX Controls are only supported by Microsoft Internet Explorer®. To access the suite of functions and types of display to which ClearSCADA's web client and your user account provides access, we recommend that you use Internet Explorer 11 to run WebX. Other web browsers provide access to a sub-set of functionality and document types. The interface layout varies slightly between browsers. The WebX documentation in the online Help explains WebX functionality that is available using Internet Explorer 11.

The main differences between a WebX client and ViewX are:


Disclaimer

ClearSCADA 2017 R3