Quick Start Tutorial
This section provides a guided tour designed to lead you through connecting a SCADAPack Eoutstation to Geo SCADA Expert, then communicating with that outstation using the DNP3 protocol. The procedure is for a SCADAPack ES outstation, however similar steps can be undertaken using other E outstation models.
To perform the procedure, you will need:
- A server and client on which Geo SCADA Expert is installed.
- A SCADAPack ES outstation and power supply.
- RS-232 9-Pin D-Sub to RJ12 Serial cable—see the SCADAPack ES Hardware User and Reference Manual for information on the construction of this cable.
- A small flat head screwdriver—to change the Hex Switch settings and tighten the I/O terminals.
- Two short lengths of insulated copper wire—to connect analog output 4 of the SCADAPack ES outstation to analog input 12.
Now proceed as follows: