Geo SCADA Expert Configuration for Hilscher Devices on DeviceNet or PROFIBUS-DP Systems
In order for Geo SCADA Expert to communicate with Hilscher devices on a DeviceNet or PROFIBUS-DP system, you need to configure:
- A Hilscher Board for each card that you want to scan on a Hilscher device (see Configuring a Hilscher Board).
- A Hilscher IO Image Scanner for each type of data that you want to scan at a different location or different scan rate on a Hilscher device (see Configuring a Hilscher Scanner).
- A Hilscher IO Image Point for each measuring instrument or control device that you want Geo SCADA Expert to monitor or control on a Hilscher device.
Choose from:
- Hilscher IO Image Analog Point (for analog input or output data)
- Hilscher IO Image Digital Point (for digital input or output data).
For more information, see Points Used on Hilscher Scanners.