Configuring Digital Points
Use OPC XML-DA Digital Points to map digital ‘point’ data on OPC XML-DA servers into Geo SCADA Expert in a format that it can understand, and vice versa.
Configure the properties of each Digital point using the fields on the OPC XML-DA Digital Point Form.
This section covers configuration of the digital-specific properties on the OPC XML-DA tab of the Form.
Use the OPC XML-DA tab to:
- Configure Common Point Properties on the OPC XML-DA Tab
- Define which Configuration Properties are Retrieved from an OPC Source.
For information the Digital Point tab on the Digital Point Form, see Defining Digital Point Details in the Geo SCADA Expert Guide to Core Point Configuration.
For information on the Control tab, see Define the Control Settings for a Digital Output Point in the Geo SCADA Expert Guide to Core Point Configuration.
For information on the Control Checks tab, see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration.
For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.