Configuring SE RPC Digital Input Points

With Geo SCADA Expert’s SE RPC driver, you use:

The SE RPC driver supports 1-bit SE RPC Digital Input points. You configure the properties of each SE RPC Digital Input point using fields on the SE RPC Digital Input Point Form.

This section covers configuration of properties on the Digital Point tab of the SE RPC Digital Input Point Form. For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.

For SE RPC Digital Input points, use the Digital Point tab to:


Disclaimer

Geo SCADA Expert 2020