Serial Communications
            For serial communications, Geo SCADA Expert uses channel(s) that have:
- An MPIvia serial adapter Connection Type, in order to communicate with the Simatic S7-300 or S7-400 series of PLCs.
 - A PPIvia serial adapter Connection Type, in order to communicate with the Simatic S7-200 series of PLCs.
 
For information on configuring either of the above Connection Types, see Configure the Connection Properties.