Minimum Configuration for a TBox Point

The following applies to TBox Analog Input Points, TBox Analog Output Points, TBox Digital Input Points, TBox Digital Output Points and TBox String Points. For the configuration of Historical Analog Points, see Configuring TBox Historical Analog Points.

For a TBox point to be capable of functioning, as a minimum you need to specify these features on the <Point Type> tab of the appropriate type:

Additionally, if the point is an output point, you need to:

If you want to store retrieved TBox Chronologies or instantaneous Sampling Tables in the server database, you need to:

If you want to store other types of retrieved TBox Sampling Tables in the server database, you need to:

Also ensure that the point and the database items on which it depends are In Service, and have saved, valid configuration. This will produce a point that is capable of functioning using the default configuration settings.


Disclaimer

Geo SCADA Expert 2020