TBox-Specific Information
This section summarises the main differences between the TBox driver and other Advanced Drivers (see the Geo SCADA Expert Guide to Advanced Drivers).
- TBox has two different methods of recording historic data. These are:
- Chronologies, which can be associated with either Digital or Analog Points
- Sampling Tables, which are associated only with Analog Points, and are handled in Geo SCADA Expert using special Historical Analog Points.
For more information on how these are used, see Historical Data Logging.
- Blocks of points (see Using Blocks of Points)
- Actions that are Specific to the TBox Driver
- TBox-Specific Status Display Attributes
- Alarms on TBox