Alarm-Related Entries in the Events List

Events Lists provide an audit trail of activity on your system. Events that are recorded in an Events List include those that relate to alarm activity. Alarm-related entries are displayed using the appropriate Severity color (see The Color of Entries in a List other than the Alarms List in the ClearSCADA Guide to Lists). In each case, the entry’s Source indicates the Group, Group Instance, or item with which the event is associated.

Alarm-related activities that are recorded in the Event Journal (Events List) include:

Further Information

Alarm Redirections and Redirection Actions: see the ClearSCADA Guide to Alarm Redirection.

Events and Events Lists: see the ClearSCADA Guide to Lists.


Disclaimer

ClearSCADA 2017 R2