Launch a ViewX Client on a Multi-Monitor Setup
You can configure the ViewX client to launch on a Multi-Monitor setup with specific interface components displayed on each monitor. By associating a Window Container with a particular monitor, you can manage the content the monitor displays.
The Startup Configuration File defines how many Window Containers are required by a Multi-Monitor setup, and the content that each displays (see Configure a Multi-Monitor Setup).
You can also use the Startup Configuration File to: