Monitor Availability

The Startup Configuration File uses the Monitor element to apply a value to each Window Container included in a Multi-Monitor setup. When the ViewX client launches, ClearSCADA matches this number with the display numbers allocated to each connected monitor by the Windows operating system.

As a result, any changes to the allocation of display numbers within the operating system will impact how the Window Containers are displayed on a Multi-Monitor setup. Window Containers may move from monitor to monitor as ClearSCADA automatically responds to any monitor availability changes detected in the operating system.

The following list describes the scenarios that will cause Windows to update the display numbers applied to a Multi-Monitor setup, and the impact this has on a ClearSCADA system.

If a monitor that is defined in the Startup Configuration File is not available when ClearSCADA launches, the following message will display:

When you select OK, any Window Containers that are configured to appear on an unavailable monitor will appear on the monitor displaying the Primary Window Container (as described above).


Disclaimer

ClearSCADA 2017 R2