Basic Configuration Procedures
You can only configure items in the ClearSCADA database if your User Account is assigned the Configure Database feature and allocated the relevant security permissions (see Database Security).
You configure some types of database item by specifying properties on the relevant configuration Form (see Working with Forms). With other types of item, you configure the item using an Editor (see Displaying an Editor).
Sections within this guide explain the procedures for:
- Adding an item to the database (see Add an Item to the Database)
- Saving Configuration Changes
- Copying a Database Item
On ClearSCADA systems that have multiple databases, you can use ClearSCADA’s Import and Export features to duplicate configurations between ClearSCADA databases that are not connected together (see Importing and Exporting Database Items). You can also copy items from one ClearSCADA database and then paste them into another (see Use Copy and Paste to Copy a Database Item).
- Moving a Database Item
- Renaming a Database Item
You can include any alphanumeric characters in the name of an item in the ClearSCADA database. However, there are limitations to the overall length of the name (including the path to that name). There are also restrictions as to which non-alphanumeric Unicode characters you can include in a name. For further information, see Naming Restrictions.
- Deleting a Database Item.
In order for outstations and their component parts (such as points) to communicate correctly with the ClearSCADA server, their database configuration has to be stored at the outstation. With some types of outstation, you can configure the data within ClearSCADA and then download that data to the outstation (see Downloading Configuration Changes). With outstations that do not support downloading, care needs to be taken to ensure that the same settings are configured in both the outstation and the ClearSCADA database.
UNEXPECTED BEHAVIOR OF APPLICATION
Where a database item references another item (for instance, a point references the outstation on which it is located), you can display a list of those references (see Displaying a Database Item’s References). Be aware of these references should you move, copy, or delete an item in your database.
Further Information
Keep a detailed record of the property changes made on your system: see Configuration Changes Auditing.