Create a Report

To add a Crystal Report to ClearSCADA:

  1. Display the Database Bar (see Display an Explorer Bar).

  2. Select the Create New option.
    A further menu is displayed.
  3. Select the Other option.
    A further menu is displayed.
  4. Select the Crystal Report option.
    A Crystal Report entry is added to the Group or System. The entry is highlighted in the Database Bar tree structure, ready for you to define its name.

  5. Enter a suitable name for the report (see Naming Restrictions in the ClearSCADA Guide to Core Configuration).
  6. Select another part of the interface or press the Enter key to confirm the entry.

You can then use the Crystal Report Form to configure the report’s properties. The Form has several tabs:

If you want to export the report, you also need to configure the relevant properties on the following tabs:

(If the report is not going to be exported, set the Export Format and Destination to ‘None’.)

If the report needs to be displayed from Original WebX clients (as opposed to WebX clients), configure the relevant properties on this tab:

For further information on configuring reports, see as appropriate:


Disclaimer

ClearSCADA 2017 R2