Configuring Digital Points

The IEC 60870-5 driver supports 1-, and 2-bit Digital Input points and Digital Output points.

Configure the properties of each digital point using the fields on the IEC 60870-5 Digital Input Point Form, or the IEC 60870-5 Digital Output Point Form, as appropriate. Each Form has several tabs.

For both IEC 60870-5 Digital Input Points and IEC 60870-5 Digital Output Points, use the Digital Point tab to:

For IEC 60870-5 Digital Input Points, also use the Digital Point tab to:

For IEC 60870-5 Digital Output Points, there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the ClearSCADA Guide to Core Point Configuration).

For information on the properties on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Advanced Drivers.


Disclaimer

ClearSCADA 2017 R2