Configuring a Map Source

A Map Source represents the origin of a layer on a ClearSCADA map. The Map Source can be online (on the internet) or offline (not on the internet). For example, a layer could be the OpenStreetMap® world map or an overlay graphic showing wind speed and direction data from an open source server. To create a map, you specify and then combine one or more Map Sources (layers) to create a Map Set, which users can then display as a multi-layered composite map. For more information, see Creating a ClearSCADA Map and see Creating a Map Set.

Each Map Source is represented in the ClearSCADA database by a Map Source database item.

ClearSCADA currently provides access to a number of different Map Sources (see Which Map Sources does ClearSCADA Support?).

To create a Map Source database item, see Creating a Map Source.

Once you have created a new Map Source item, you then need to define its settings. To do this, right-click on the item to display its Object Menu then select the Edit Properties option.

ClearSCADA will then display the Map Source form:

This section describes the settings on the Map Source tab of the Map Source form.

You can find details of the settings on the other tabs as follows:

Use the Map Source tab to set the various properties of a Map Source. Each source has different settings such as:

For more information, there is a topic for each of the standard ClearSCADA Map Sources. Select the appropriate topic in the gray footer section at the bottom of this topic.


Disclaimer

ClearSCADA 2017 R2