Editing a Pie Chart

When you have added a pie chart to a Mimic, you can access its Pie Chart Properties window to edit its settings. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)

The Pie Chart Properties window contains two tabs:

To remove a slice from a pie chart, you should set the value of the animation for the slice to 0 before you clear it (remove the slice). If you do not set the slice animation to 0, the pie chart will continue to show the slice, even after you have cleared the animation for the slice. This is because the pie chart will maintain the previous value of the slice.


Disclaimer

ClearSCADA 2017 R2