Specify a Trip Sequence for an SQL Export Object

You can use an Object trip sequence to specify information about the SQL Export database item itself. This type of trip sequence can be used to include information on:

 

To specify the trip sequence for a SQL Export Object, you enter the trip code:

%O<field>[.<field>][;<format>]%

where:

the first <field> is one of the following:

 

If <field> is a reference field or an aggregate field, then you can include further <field>(s) in the trip sequence, in order to specify further database item(s), that are themselves referenced by the database item listed in the preceding <field>.

Use the final <field> in the trip sequence to specify the required Configuration or Data field (OPC property) in the database item or aggregate that is specified in the preceding <field>.

 

<format> is optional and can be used to control the appearance of the information that ClearSCADA substitutes in place of the Object’s trip sequence. You only need to specify a format if:

or if:

The custom formats that you can specify for an Object field are the standard custom value formats that are supported by ClearSCADA (see Date and Time Syntax, see Numeric Syntax, see Text String Syntax, and see Boolean Syntax—all are sections in the ClearSCADA Guide to Core Configuration).

 

You can ascertain the configuration, data, reference, and aggregate fields that you can specify using an Object trip sequence, along with an indication of each field’s type, using either of the following:

You can also click on the relevant configuration field on a Form and observe its name and type in the Status Bar. (Remember that a field’s name often differs from the label that is shown for that field on the configuration Form. (The label is displayed in the language that is associated with the logged on user’s specified Locale.) It is a field’s name, rather than its label, that has to be specified in any Object trip sequence.) Data fields (and some Configuration fields, such as ParentGroupName) are not displayed on configuration Forms—use the database Schema or OPC Data Bar to ascertain information about such fields.

Example:

%OParentGroupId.Name%
(Provides the name of the Group or Group Instance in which the SQL Export is located. For instance, ‘Zone 1’, for an SQL Export that is located in the Group ‘Zone 1’.)

%OParentGroupId.ParentGroupId.FullName%
(Provides the full name (including the path) of the SQL Export’s ‘grandparent’ Group or Group Instance—the Group or Group Instance in which the SQL Export’s Group or Group Instance is located. For instance, ‘My Database.Eastern Region’, for an SQL Export that is located in the Group ‘Zone 1’, which itself is within the Group ‘Eastern Region’. (With ‘Eastern Region’ being in the Group ‘My Database’.))

%OAlarmRedirection.Trigger1%
(Provides the value of the Trigger1 property. ‘AlarmRedirection’ is the name of the field that links to the SQL Export’s Alarm Redirection aggregate. Trigger1 defines the first Trigger State on the Alarm Redirection aggregate. (On the Redirection tab, ‘Trigger State’ is the label that identifies the column of trigger state fields—the label is displayed in the language that is associated with the logged on user’s specified Locale.) This trip sequence can only be used if an SQL Export has Alarm Redirection enabled.)

%OId;000000%
(Provides the SQL Export item’s Id—the number that uniquely identifies the SQL Export item in the ClearSCADA database. The 00000 formatting is included to force the Id to be displayed as a series of five digits (if the Id is smaller then five digits, it will be preceded by one or more zeros).)


Disclaimer

ClearSCADA 2017 R2