Configuring Digital Points

The Sofrel driver supports 1-, 2-, and 3-bit Digital Input points and Digital Output points.

Configure the properties for each Digital point using the fields on the Digital Input Point Form, or the Digital Output Point Form, as appropriate.

This section covers configuration of properties on the Digital Point tab of both Digital Point Forms, and the properties on the Control tab for Digital Output points. The properties on other tabs are common to points on many advance drivers (see Tabs on Point Forms).

Use the Digital Point tab to:

For Digital Output Points, use the Control tab to:

Use the Control Checks tab to:


Disclaimer

ClearSCADA 2017 R2