Customize the WebX Interface

Your User Account settings determine the initial layout and availability of components in the WebX window. For example:

Your User Account settings also determine how much you can interact with the Alarm Banner. For example:

When using the WebX interface, you can:

Providing that your User Account has the relevant settings enabled, you can arrange the windows in the WebX interface to suit your preferences. The available arrangement options are described in the following topics:

(The links above, other than the first one, are to topics.)

Further Information

Customize the ViewX Interface.

User account setup: see Creating a User Account.


Disclaimer

ClearSCADA 2017 R2