Set Token

Associated with: Wonderware Historian database items on which the Historian is specified as 'AVEVA Insight (Wonderware Online)'

Security permission required to access this pick action: Configure

Before you can connect ClearSCADA to AVEVA Insight (formerly Wonderware Online), you need to enter a connection token in ClearSCADA. The token contains information needed to help secure the communications between the two applications. Before you can enter a token, you first need to generate one by using AVEVA Insight Publisher (formerly Wonderware Historian Publisher) (see Generate a Connection Token with AVEVA Insight Publisher).


Disclaimer

ClearSCADA 2017 R2