Introduction to the Hilscher Driver

This driver is a simple driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is designed for use by engineers who are responsible for configuring Geo SCADA Expert to communicate with HilscherTM products. System administrators can also use this guide when investigating unexpected conditions related to the Hilscher driver.

Document Scope

This guide explains how to configure Geo SCADA Expert to communicate with HilscherTM products that use PROFIBUS-FMS®, PROFIBUS-DP®, and DeviceNetTM. It also explains how to use the driver features for fault finding on the system.

HilscherTM produce various products designed for use with fieldbus technology and for communications using one of several industrial fieldbus networks. The driver enables Geo SCADA Expert to transmit data to and from Hilscher devices, where those devices use one of the following fieldbus control networks:

The Hilscher Driver documentation explains how to configure Hilscher-specific features and items within the Geo SCADA Expert database (see Configuring Geo SCADA Expert to Communicate with Hilscher Devices).

It also explains driver-specific aspects that may be of interest to System Administrators and engineers when investigating any unexpected system behavior (see Hilscher Specific Status Display Attributes).

For Hilscher, PROFIBUS, or DeviceNet information not covered by this guide, see the relevant Hilscher or fieldbus documentation.

NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).


Disclaimer

Geo SCADA Expert 2019