Understand Events Lists

The Events List displays a row of values for each event that occurs in your Geo SCADA Expert system, and uses columns to separate and categorize the values. The column headings indicate what the values in each column represent. The columns that are displayed on your Events List can be configured by a system administrator (see Events Journal List Settings).

NOTICE

LOSS OF DATA

There is a limit to the number of Event Journal records per database item per hour that can be logged. If the number of records for an individual item reaches this limit an alarm is raised to indicate that the granule has reached the maximum value and no more events will be logged for the item for the remainder of this period. This will result in the loss of data that has been discarded. To help prevent loss of data, you need to set appropriate maximum values, see Define the Acceptable Number of Event Journal Records.
Failure to follow these instructions can result in loss of data

The default column headings for the Events List are:

Severity

Events have a severity level that indicates the importance of the event. Severity for events works in exactly the same way as Severity for alarms and has the same range of severity levels (see Alarm Severity).

Time

The date and time at which the event was recorded. Events have both an ‘occurrence time’ and a ‘received time’. Whenever the Geo SCADA Expert server provides the time stamp, these times are one and the same. Whenever Geo SCADA Expert receives a time stamped event from an outstation, the Time column displays that record’s ‘occurrence time’ (the time stamp provided by the outstation or scanner).

Events that are generated at the master station (Geo SCADA Expert) are time stamped by the server. If an event occurs at the outstation, the time stamp of that event depends on the driver. With some drivers, the outstation time stamps the data and then passes that data to Geo SCADA Expert. With other drivers, the time stamp might be generated by the outstation or the server, depending how the data was reported. Outstations on some drivers do not support time stamping of data, and therefore the server time stamps that data when it receives it from the outstation.

Source

The name of the item with which the event is associated. The Source is not always the name of an item in the Geo SCADA Expert database. For items that are in the Geo SCADA Expert database, the FullName of the item is displayed.

Message

A short text description of the system occurrence that caused the event to be generated.

User

The identity of the user that caused the event to be generated. Users include:

<User Name>

The name of a user that is logged on to Geo SCADA Expert and whose activity caused an event to be generated. <User Name> generated activities might include, for example, logging on and off Geo SCADA Expert, modifying an item’s configuration, or sending controls to plant.

Guest

This is a built-in user account that is disabled on new Geo SCADA Expert installations by default. Events are assigned to the Guest user should someone perform activities on a ViewX Client without being logged onto Geo SCADA Expert via that client. Guest user access is typically restricted to help prevent unauthorized interaction with the system.

Web

This is a built-in user account that can only be used with Original WebX clients (as opposed to Virtual ViewX clients). Events are assigned to the Web user should someone perform activities on an Original WebX client without being logged onto Geo SCADA Expert via that client. Web user access is typically restricted to help prevent unauthorized interaction with the system. (Unlike Original WebX clients, you do need to log on to a Virtual ViewX client in order to interact with Geo SCADA Expert.)

<Super User Name>

If enabled on your system, the Super User account provides access to all Geo SCADA Expert features. The account is typically used to initially set up Geo SCADA Expert and is then typically removed once appropriate administrator-level user accounts have been set up.

For more information on any of the above users, see User Accounts.

If the event was not caused by ‘user’ interaction, there will be no entry in this column.

Category

Each event has a category that indicates the type of event. This allows you to filter the Events List so that it only displays events of a specific category, such as outstation communications events (see Add a Filter to a List).

The event categories include:

Action

The event was logged due to an action being performed. An action can be triggered manually by an operator, or automatically—for instance, by a Method Call, Logic, or a Schedule.

Alarm Analysis

The event was logged due to the permitted time for either receiving, responding to, or clearing an alarm being exceeded. Alarm Analysis periods can optionally be configured for Severity ranges (see Add a Severity Range).

Alarm Redirection

The event was logged due to an alarm being redirected (as part of the Alarm Redirection feature that allows, for example, alarms to be sent to pagers).

Archive Volume

The event was logged due to a detected problem associated with either deleting, duplicating, or recreating an archive volume (the media to which data is being archived). For example, the archive volume being full.

Archiving

The event was logged due to data being archived, for instance onto hard disk, CD, DVD, or compact flash. Archiving provides the ability to store historic and/or event data offline. For more information on archiving, see Archiving.

Backup

The event was logged due to an operation associated with a database Backup item. For example, an event is logged whenever a backup is initiated

Callback

The event was generated due to a successful callback, an unsuccessful callback, or an unexpected callback. (The callback feature allows you to send a message to an outstation to instruct it to dial in. The outstation should then report its data within a specific amount of time).

Channel Status

The event is associated with a communications channel’s status. For example, an event is logged if channel communications is interrupted unexpectedly (an alarm is also raised).

Comment

The event was logged due to a comment being created (see Insert a Comment for an Event).

Configuration

The event was logged due to configuration changes being made (for example, a new item being created, the configuration of an existing item being modified, an item being renamed or deleted from the database).

If you have the Configuration Changes feature enabled on your system, you can keep a detailed record of any configuration changes. You can use the Property Change History List to view a summary of the configuration changes on your system (see Display a List of Property Changes).

Control Checks

The event was logged because a Control Feedback point or an Uncommanded Change point did not have a required value (see Control Feedback Settings and see Uncommanded Change Settings).

Control Status

The event was logged due to both successful and unsuccessful control activity. For example, a control request, or execution.

Database Server

This category is used for miscellaneous events associated with server activity. For example, an event logged due to unexpected activity occurring while receiving a request from a ViewX or Virtual ViewX client.

Dial In Overactive

The event has been logged due to a PSTN outstation dialing in more often than expected.

File Upload Status

The event is associated with file upload activity, for example, outstation data being uploaded to Geo SCADA Expert. Where supported by a driver, if the system set-up does not allow Geo SCADA Expert to communicate with one or more outstations, file uploading can be used to upload the data from those outstations to Geo SCADA Expert.

Forecast

The event is associated with a Forecast item. For example, an event is logged if an alarm is raised due to a Forecast from an external application having values that are outside the alarm limits for the Forecast item in Geo SCADA Expert.

Historic

The event was logged due to an operation associated with historic data (for example, historic data being inserted, or modified).

Historic Corrupt

The event was logged due to an alarm raised to indicate errors detected in historic data that is being retrieved.

Historic Export

The event was logged due to an operation associated with the export of historic data from Geo SCADA Expert.

Historic Overactive

The event was logged due to an alarm raised to indicate that the value of the maximum number of records per data file (granule) exceeds one of the historic limits set.

Historic Write Error

The event was logged due to an alarms raised to indicate write errors detected when historic data is being recorded.

Interface Alarm

The event was logged due to an external application raising an alarm using the SetInterfaceAlarm method. The SetInterfaceAlarm method is purely for use with the Automation Interface. For more information, see the database Schema.

Interface Event

The event was generated by an external application, using the SetInterfaceEvent method. The SetInterfaceEvent method is purely for use with the Automation Interface. For more information, see the database Schema.

Outstation Comms

The event was logged due to a change in outstation communications status (for example, due to an incoming call).

Outstation Driver Timeout

The event was logged due to a request from an advanced driver timing out internally. For example, an event is logged if a request fails to complete within the Scanner Command Timeout duration (see Define the Scanner Command and Request Timeouts).

Outstation Error

The event was generated when a general outstation error was detected (an outstation error that is not included in the Outstation Hardware or Outstation Comms categories).

Outstation Hardware

The event is associated with the status of the outstation’s hardware.

Outstation Status

The event is associated with the status of an outstation. For example, an event can be logged when an outstation is reset, or when an outstation requests configuration.

Pager Comms

The event is associated with the communications status of a pager service. For example, an event is logged when there is an attempt to connect with a pager.

Point Error

The event has been logged due to a miscellaneous error associated with a point being detected.

Point No Change

The event has been logged due to a point’s value not having changed by a specified amount for a defined period of time. Such events can only be logged for points that are configured to use the No Change feature.

Point Significant Change

The event is associated with a significant change in the value of a point. This type of event can only be logged for points that are configured to use the Significant Change feature.

Point State

The event has been logged due to a point changing state. The point states are those that are defined in the configuration of each point.

Point Status

The event is associated with the status of a point. These are miscellaneous events that are not covered by Point State.

PSTN Test

The event has been logged due to a Test PSTN Connection request on a multi-drop outstation.

Scanner Status

The event is associated with a scanner or a point source (simple drivers). For example, an event is logged when an alarm is raised due to a scanner error being detected.

Scheduled Dial In

The event has been logged due to a successful scheduled dial in, an unsuccessful scheduled dial in, or an unexpected scheduled dial in.

Server Status

The event is associated with the status of a server or channel (simple drivers). For example, an event is logged when there is a switch from one channel to another.

Set Status

The event is associated with the status of an outstation set. For example, an event is logged if the outstation set switches from one communications channel to another (switches lines).

System

The event has been logged due to an occurrence that affects the entire system, such as the server being stopped and restarted. The System category is also used for miscellaneous events that are not suited to the other categories.

System Alarm

The event has been logged due to a system-wide problem being detected, such as licenses expiring.

Text Message

The event has been logged due to a Geo SCADA Expert Server receiving a text message from an outstation or another Geo SCADA Expert server.

Unknown Dial In

The event has been logged due to an unknown PSTN outstation dialing-in to Geo SCADA Expert.

Related Topics Link IconFurther Information


Disclaimer

Geo SCADA Expert 2019