Introduction to the TBox Driver

This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring TBox items and features in the Geo SCADA Expert database.

The guide also contains information for maintenance engineers.

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s TBox driver. The TBox driver enables Geo SCADA Expert to communicate with TBox RTUs using the Modbus/TComm protocol suite.

TBox is a range of RTUs produced by CSE Semaphore. TBox combines alarm notification, data logging, integral web server, IP telemetry, and programmable automation.

The TBox driver communicates with Geo SCADA Expert using a protocol called TComm, which incorporates the Modbus protocol with extensions specifically for TBox functionality.

This guide covers the functions of Geo SCADA Expert controlling the TBox using TComm version 4.3.0.247. The TBox driver allows a Geo SCADA Expert system to retrieve data from, and control points on, TBox RTUs.

The TBox driver documentation explains:

The documentation also covers driver-specific aspects that are of interest to system administrators and engineers when investigating unexpected behavior relating to the TBox driver. For information, see:


Disclaimer

Geo SCADA Expert 2019