Introduction to the Wonderware eDNA Historian Driver

This driver is a stand-alone driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported systems or devices. To interact successfully with such systems or devices, you need to:

Intended Audience

This guide is designed to be used by engineer-level users who are responsible for configuring Geo SCADA Expert to export Geo SCADA Expert historic data to a Wonderware eDNA Historian server.

The guide also contains information for:

Document Scope

This guide explains how to configure and operate your Geo SCADA Expert system so that it can export Geo SCADA Expert historic data to a Wonderware eDNA Historian server.

The Wonderware eDNA Historian driver enables you to export Geo SCADA Expert historic data to a Wonderware eDNA Historian server.

When you have installed the driver, you can then configure a Geo SCADA Expert point or accumulator so that Geo SCADA Expert can export its data to a Wonderware eDNA Historian. Geo SCADA Expert will automatically start exporting new data for an enabled point or accumulator to the Historian. It does this by using an API called eDNALinkMx.

Geo SCADA Expert sends historic data to eDNALinkMx, which then manages its onward transmission to the Wonderware eDNA Historian. Geo SCADA Expert exports historic data at the same time as it stores the data in the Geo SCADA Expert database. It only exports newly created historic data. It will not export data that was created before you place the Wonderware eDNA Historian database item 'in service'. Geo SCADA Expert will not export data that it did not store due to historic compression or filtering (see Historic Data Compression in the Geo SCADA Expert Guide to Core Point Configuration). eDNALinkMx applies no further filtering.

eDNALinkMx can store exported historic data in a cache. This is useful if the network connection to the Wonderware eDNA Historian is intermittent or unavailable. In such a situation, eDNALinkMx will cache the export data and when the link becomes available again, it will send it to the Wonderware eDNA Historian. For more information about eDNALinkMx, see the Wonderware eDNA Historian documentation.

For each enabled point or accumulator, Geo SCADA Expert uses eDNALinkMx to create a new Object ID in the Wonderware eDNA Historian. It does this when it exports the first data to the Historian.

To export historic data to a Wonderware eDNA Historian, follow this procedure:

  1. Install the Wonderware eDNA Historian Driver.
  2. Configure the Wonderware eDNA Historian Server Setting to set up the cache.
  3. Add a Wonderware eDNA Historian Database Item to the Geo SCADA Expert database. This item holds the Wonderware eDNA Historian export settings.
  4. Configure a Wonderware eDNA Historian Database Item.
  5. Place the Wonderware eDNA Historian database item In Service.
  6. Configure the Historic details for each point or accumulator for which you want to export historic data (see Defining Historic Details for a Point in the Geo SCADA Expert Guide to Core Point Configuration).

    Historic data is only exported for points and accumulators for which a Wonderware eDNA Historian database item is specified in Export section of the configuration Form. Data that is subsequently stored in the Geo SCADA Expert historian will be exported to the specified Wonderware eDNA Historian servers. For more information about both of these requirements, see Define the Historic Export Details in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2019