SCADAPack x70

Quick Start Tutorial

This section provides a guided tour to lead you through connecting a SCADAPack 575 device to Geo SCADA Expert, and then communicating with that device using the DNP3 protocol. Although the procedure is for a SCADAPack 575, similar steps can be undertaken for other SCADAPack x70 models.

To perform the tutorial, you will need:

Proceed as follows:

  1. Confirm that the Relevant Geo SCADA Expert Components are Installed.
  2. Configure the Required Network Settings on the Computer.
  3. Set Up the SCADAPack 575 Device.
  4. Create the Required Database Items.
  5. Download Configuration to the SCADAPack 575 Device.
  6. Control the Analog Output Point.

Disclaimer

Geo SCADA Expert 2020