Configuring a WITS Counter Point

In Geo SCADA Expert, you use a WITS Counter Point database item to represent a Counter point in a WITS Field Device. You typically use a Counter Point to count pulses on a physical binary input, or to accumulate internally calculated values.

WITS Counter Point database items have a combination of configuration properties that are:

To configure a WITS Counter Point database item, you use the WITS Counter Point Form.

The configuration Form contains many fields, organized into tabs. Most of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

The Counter Point tab contains properties that are specific to WITS. Use the fields on the tab to:

When you have completed the point's configuration, you need to download the configuration to the Field Device by using the Outstation database item's Download Configuration (WITS Outstation) action. If your Field Device does not support configuration download, you will need to make the same changes to the Field Device's configuration locally.


Disclaimer

Geo SCADA Expert 2021