Configuring Advanced OPC Analog Points

Use an Advanced OPC Analog Point to map an item within the OPC DA server to an analog point in the Geo SCADA Expertdatabase. The item needs to have a suitable data type for an analog point.

Configure the properties of each analog point using the fields on the Advanced OPC Analog Point Form.

This section covers configuration of the analog-specific properties on the Analog Point tab of the Form.

Use the Analog Point tab to:

For information on the Control tab, see Define the Control Settings for an Analog Output Point and see Update an Output Point Value on Successful Action.

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).

Properties on other tabs are common to many points, see Tabs on Point Forms in the Geo SCADA ExpertGuide to Advanced Drivers.


Disclaimer

Geo SCADA Expert 2022