Installation on ViewX Clients on Which You Want to Edit Reports
On the ViewX clients on which you want to edit reports on your system, you need to:
- Install the software for the third-party Crystal Reports application. Geo SCADA Expert can interface with SAP Crystal Reports 2016 or SAP Crystal Reports 2020.
- Install the latest Crystal Reports service pack from SAP.
- Install the Geo SCADA Expert software, including:
- The relevant SAP Crystal Reports runtime engine for .NET Framework components (see Geo SCADA Expert Prerequisite Components in the Geo SCADA Expert Installation Guide)
- The ViewX Client Crystal Reports component
- The Data Access component.
- Add an ODBC Data Source Name (DSN) to allow Crystal Reports to access the Geo SCADA Expert database. Crystal Reports uses the DSN to access the relevant database whenever you create or edit a report on a client.
The DSN on a client can be either a System DSN or a User DSN. (A System DSN is shared by all Windows Users on a machine; a User DSN is specific to an individual Windows User—the user that was logged on when the DSN was added.)
We advise that the same data source name is used throughout your system, even if Crystal Reports is only to access the Local Database. (The Local Database is the Geo SCADA Expert database that contains the report.) By using the same data source name, you allow your reports to be fully portable - they can be edited from any client on which Geo SCADA Expert and Crystal Reports are installed.
(If any of your reports are to access Multiple Databases, the same data source name has to be used throughout your system—see step 5.)
Be aware that the 32-bit and 64-bit versions of the ODBC Data Source Administrator Tool display both 32-bit and 64-bit DSNs on computers that are running 64-bit operating systems.
If you are using SAP Crystal Reports 2020, you have to add a 64-bit ODBC DSN (as that version of SAP Crystal Reports is a 64-bit application).
If you are using SAP Crystal Reports 2016, even though your computer is running a 64-bit version of Windows®, you have to add a 32-bit ODBC DSN, as that version of SAP Crystal Reports is a 32-bit application.
You also have to run the 32-bit version of the ODBC Data Source Administrator Tool. To access this, enter the text ODBC Data Sources in the search box next to the Start button in Windows® and then select the 32-bit option.
For more information on setting up an ODBC DSN, see Configure an ODBC Client - System Connection using a DSN in the Geo SCADA Expert Guide to Client Administration.
- If any of your reports are to access more than one database, repeat step 4 as required, in order to add one ODBC DSN for each additional database.
In order for Crystal Reports to access multiple databases, each DSN that you add has to have the same name on both the client(s) on which the reports are to be created, and on the server(s) that will be used to generate those reports.
For Crystal Reports to access the data from other databases, the relevant reports have to be configured to access Remote Database(s) (see Specify the Data Source).
- Repeat the above steps on each Geo SCADA Expert client that is to be used for editing reports.
Further Information
For diagrams that illustrate the location of the Geo SCADA Expert components that you need to install, see Geo SCADA Expert Software Components.