Status Attributes Associated with Channels on Advanced Drivers
            The channels on advanced drivers support a combination of these status attributes:
- Id
 - Full Name
 - Type
 - Position
 - Created—(New channels only)
 - Last Modified
 - Configuration Change CRC—(Only displayed if this feature is enabled on your system)
 - Exclusive Control User—(Only channels that are under Exclusive Control)
 - Alarm State
 - Alarm Last Updated
 - Scan Status Alarm—(Channels on some advanced drivers)
 - State Alarm
 - Alarm Count
 - Suppression Status—(Channels on which Alarm Suppression is configured)
 - Suppressing Parent—(Channels on which alarms are currently suppressed)
 - Source
 - State
 - Last Updated
 - Quality
 - IO Logging
 - Serial Port Statistics—(Channels with serial connections only)
 - Comms Logging
 - Telnet
 - Comms Statistics
 - Message Count
 - Scan Quality—(Direct channels only)
 - Incoming Calls—(PSTN channels only)
 - Outgoing Calls—(PSTN channels only)
 - Outgoing Call Quality Factor—(PSTN channels that are selected for use by their call quality factor).
 
For information on channel status attributes that are not listed above, see the driver-specific documentation.