Status Attributes Associated with Scanners on Simple Drivers
The scanners on simple drivers support a combination of these status attributes:
- Id
- Full Name
- Type
- Position
- Created—(New scanners only)
- Last Modified
- Configuration Change CRC—(Only displayed if this feature is enabled on your system)
- Exclusive Control User—(Only scanners that are under Exclusive Control)
- Alarm State
- Alarm Last Updated
- State Alarm
- Alarm Count
- Suppression Status—(Scanners on which Alarm Suppression is configured)
- Suppressing Parent—(Scanners on which alarms are currently suppressed)
- Source Name
- Source
- State
- Last Updated
- Quality
- Point Statistics
- Comms Statistics.
For information on scanner status attributes that are not listed above, see the driver-specific documentation.