Configure an AVEVA Historic Data Export Item

To configure a database item that represents a connection to a historian in an AVEVA application, you have to display the AVEVA Historic Data Export Form (see Display a Form) and configure the relevant settings on that Form.

The Form has several tabs:

Use the fields on the AVEVA Historic Data Export tab to define the connection properties that enable Geo SCADA Expert to communicate with the historian server:

For information about configuring properties in the Tag Names, Connection, and Store/Forward sections of the AVEVA Historic Data Export tab, see the relevant topics in this section. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

Specify the points and/or accumulators for which you want to export historic data using the AVEVA Historic Data Export item: see Define the Historic Export Details in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2022