Historian Tags

A tag in a historian in an AVEVA application is the equivalent of a point or accumulator in Geo SCADA Expert.

Geo SCADA Expert automatically uses HCAL to create a new tag in that historian when it first exports data for the point or accumulator. In order for Geo SCADA Expert to export historic data:

Tag creation is triggered when the first historic data for the point or accumulator is added to Geo SCADA Expert's historian after the AVEVA historian had been specified as the historian application to which the point or accumulator data is to be exported. Data is only added to Geo SCADA Expert's historian if it meets the historic storage criteria for that point or accumulator. This includes meeting any Compression and/or Historic Data Filter criteria that might be configured for that point or accumulator. For more information see:

When Geo SCADA Expert uses HCAL to create a new tag in the AVEVA application's historian, Geo SCADA Expert gives the tag a name. The content that is included in the name depends on whether a Prefix is specified, and whether the Aggregate Name Suffix check box is selected on the AVEVA Historic Data Export Form (see Specify the Properties that are Associated with Tag Names).

The tag name has the following format:

[<prefix>.]<object name>[.<aggregate name>]

(where [<prefix>.] and [.<aggregate name>] are optional)

 

The tag name for a single point, named 'Internal Analog Point' in Geo SCADA Expert, varies, depending whether the Prefix or Aggregate Name Suffix are used:

Internal Analog Point
(if neither the Prefix or Aggregate Name Suffix are used)

CS.Internal Analog Point
(if the Prefix is used, but the Aggregate Name Suffix check box is clear)

CS.Internal Analog Point.Historic
(if the Prefix is used and the Aggregate Name Suffix check box is selected)

Internal Analog Point.Historic
(if no Prefix is specified, but the Aggregate Name Suffix check box is selected)

A tag name can be a maximum of 256 characters in length. Ensure that the prefix and object names are not too long. For more about the tag name's Prefix and Aggregate Name Suffix, see Specify the Properties that are Associated with Tag Names.

Tags also have a description associated with them. By default, Geo SCADA Expert sets the description to the class name and object ID of the point or accumulator. This is so that you can match tags in the AVEVA application's historian with items in the Geo SCADA Expert database, for example, after renaming an item in Geo SCADA Expert (see Troubleshooting Historic Data Export Operation). If you do not want to use the default description, you can change it by creating a custom Geo SCADA Expert metadata field to configure the TagDescription property (see Configure Historian Tag Properties from Geo SCADA Expert and see TagDescription).

If you do one of the following in Geo SCADA Expert:

Geo SCADA Expert will use HCAL to delete the tag from each historian server.

If you modify a point or accumulator to remove a historic export, Geo SCADA Expert will use HCAL to delete the tag from the historian server for each removed export.

If you change the tag prefix in Geo SCADA Expert, then Geo SCADA Expert will only apply the new prefix to points or accumulators:

All existing points and accumulators will retain their existing tag names, unless you use the RenameTag method to realign the tag names with the names of the points or accumulators with which those tags are associated.

If you move or rename points or accumulators in Geo SCADA Expert (or a group containing points or accumulators) then these points or accumulators will retain their existing tag names. (However, with some versions of AVEVA Historian (as opposed to AVEVA Insight), you can use the RenameTag method to realign the two names. See the topic about the method for information about which versions of AVEVA Historian support the RenameTag method.)

To update the name of a tag in AVEVA Insight (formerly Wonderware Online) and older versions of AVEVA Historian (formerly Wonderware Historian), do one of the following:

If you do either of these, Geo SCADA Expert will use HCAL to:

NOTICE

LOSS OF EXPORTED HISTORIC DATA

If you follow the above procedure to update a tag name, you will lose all of the exported historic data associated with the tag.
Following the above procedure will result in the loss of exported historic data.

You can use the Status display to view the tag names associated with each point or accumulator (see Status Attributes that are Specific to the AVEVA Historic Data Export Driver).


Disclaimer

Geo SCADA Expert 2022