Configure Historian Tag Properties from Geo SCADA Expert

Each historian tag has a set of properties. You can configure these properties from Geo SCADA Expert by creating custom metadata fields which are mapped onto the tag properties. For some properties, Geo SCADA Expert will automatically configure the property with a default value. For example, Geo SCADA Expert will configure the EngineeringUnit property with the Units for analog and counter points. However, you can override this default by defining a custom metadata field for the property.

You cannot configure some properties. Their values are fixed by Geo SCADA Expert or HCAL.

When Geo SCADA Expert creates a tag in a historian, it automatically configures the tag’s properties. It uses the metadata field values of the point or accumulator. If you change a metadata field value that is mapped onto a tag property after a user has created the tag, then Geo SCADA Expert will either update the tag:

To create a metadata field in Geo SCADA Expert, use the Metadata Window to Add or Modify an Extra Field.

When Geo SCADA Expert prompts you to select the type of field that you want to add, select Standard.

The Edit Field window is displayed.

Enter the following:

For details about the other fields in the window, see Add or Modify an Extra Field in the Geo SCADA Expert Guide to Server Administration.

You can map a Geo SCADA Expert metadata field to each of the predefined tag properties listed below. Follow the links for more details about these properties, including theType that you need to enter in the Edit Data Field window when you create the metadata field. The information also includes the default value of each predefined tag property in the historian. Geo SCADA Expert will overwrite this default value if you create a metadata field for the tag property.

The following are predefined tag properties in the historian that have fixed values. If you create a Geo SCADA Expert metadata field for any of these properties, Geo SCADA Expert will log an error and will not use the metadata field.

The following are the predefined tag properties in the historian that either do not apply or are not useful in Geo SCADA Expert. If you create and configure a Geo SCADA Expert metadata field for any of these tag properties, the tag property will retain its value regardless.

Further Information

Historian Tags.


Disclaimer

Geo SCADA Expert 2022