SCADAPack Modbus Realflo Controller Status Attributes

This driver is an extension driver. As such, it supports a combination of the status attributes that are supported by its 'parent' driver, in addition to its own driver-specific status attributes. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the status attributes that are supported by this extension driver.

In addition to SCADAPack Modbus Controller Status Attributes, Realflo-enabled SCADAPack controllers support the following Realflo-specific status attributes:

 


Disclaimer

Geo SCADA Expert 2022