Choose Setup Type

You can use the Geo SCADA Expert Installer’s Choose Setup Type page to choose from up to three different types of installation:

The Full (Recommended) option is only offered on Server and Server and Clients installations. Likewise, the Typical and Custom options only offer server components on Server and Server and Clients installations. With such installations, you have to install the Local Web Proxy Part 1/2 (IIS) and Local Web Proxy Part 2/2 (ARR) prerequisites (see Geo SCADA Expert Prerequisite Components). If these prerequisites are required, but have not yet been installed, use the Back button on the Installation Wizard pages to go back to the Setup page and select the required prerequisites from that page.

Full (Recommended)

Select Full (Recommended) to install Geo SCADA Expert server, Geo SCADA Expert Client, and Data Access components. The Full installation also includes example projects and many, but not all, of the supported drivers.

You can find out which components are included in Full Install.

Typical

Select Typical to install the most commonly used components for:

You can make your selection on the Typical Install page (see Typical Install).

Custom

Select Custom if you want to choose which components will be installed. You can make your selections on the Custom Setup page.

You have to use Custom if you want to install different components to those included in the Full or Typical installations.

Further Information

Example Projects.


Disclaimer

Geo SCADA Expert 2022